I have a problem with bq2002T NiMH fast-charge management IC. It does provide enough voltage but not the amp. It started at 120mA at 12 V once I connect it to a 12V power supply, and it will keep dropping to less than 10mA. Is this normal? Obviously, the battery was not charged due to very little juice. I am wondering if I should l charge 12V NiMH battery with more than 12V. I saw the spec saying up to 25 V or 18+Vbat? I did try 24V power supply, the amp started at 1200mA and then kept dropping down. Is this normal?