Other Parts Discussed in Thread: PTH08080W
Hi
I have designed a small 5V Power Module using a PTH08080W Module.
PTH08080W is showing strange behavior, whenever I turn on the power supply (~11V), the output instead of quickly going to 5V, slowly climbs its way taking around 30-45seconds. Sometimes, the output simply get stuck between 3-4V. At this point, if touch the PCB with my fingers, the output instantly jumps to 5V. Also, if I turn on the power while touching the PCB, the output quickly goes to 5V.
The input capacitor is a 100uF/25V electrolytic. On the output, there's a 100uF/10 electrolytic, a 0.1uF and a 10nF capacitor. Does anybody know exactly what is wrong here? I can put up the PCB design if necessary.