Hi.
I'm normally not designing power-related circuitry, but now I'm considering the using the TPS23754 in a design. I have tried to read the spec, but I'm still not sure about the output levels and how it's adjusted.
I need to generate a +24V system voltage (1A max current), from the ethernet cable. Is this voltage level achievable, and what transformer should I use?
I'm planning on implementing this feature on a Gigabit LAN. Do you seee any problems with that?