Dear TI engineer
I've tested my 3kW DC-DC converter with your ucc28950 PWM IC.
However, currently I have unanymous problem.
At light load condition, Output C/D duty was not 50 to 50% but asymmetric ducy cycle.
I found application report ; slua275 ucc3895 OUTC/D asymmetric dyty cycle operation.
Plz check below questions
1. Detail logic block described in in ucc28950 datasheet is the same as which of ucc2895?
2. In slua275, it metioned, " Also, when using synchronous rectifiers in current mode operation this problem does not typically exist due to the additional reflected secondary current added to the primary side current sense.'. I couldn't understand why? Can you explain in datai?
3. Recommand me to escape this problem.. ( ramp pin is already located inside the PWM IC, I couldn't find any external method which you used in slua275.