Other Parts Discussed in Thread: TPS63001
Hi,
My customer applied TPS63001 to the Wi-fi chip power in Mobile Router.
Before apply TPS63001, They used XC9236. (step down converter)
Problem is TPS63001 current consumption.
They checked Mobile Router’s current consumption when used XC9236, TPS63001 PS mode enable, TPS63001 PS mode Disable.
They expect the same current consumption result when using TPS63001 and XC9236.
But, result is more higher than XC9236 When using TPS63001 PS enable/disable
Mobile Router set status current consumption as below: (PS enable : connect to GND with PS/Sync pin / PS disable : connect to Vin with PS/Sync pin)
|
|
Sleep mode Current |
Operating mode Current |
|
XC9236 |
2mA |
105mA |
|
TPS63001 PS enable |
2.7mA |
180mA |
|
TPS63001 PS disable |
6mA |
105mA |
I have a question as below
-
Is this situation is right?
-
They can’t assigned GPIO. So, Do you have a method that current consumption performance like as XC9236 without GPIO control?
-
Can you recommend to me any other component? It must be Pin to Pin with TSP63001.
Best Regards,
DH.