1. It seems the internal temp sensor is drifting, depending on charge or discharge current. Temp seems proportional to magnitude and direction of current flow. Discharge current drives temp down and charge current drives temp up. What could cause this? The readings of voltage and current seem to be highly accurate. It is connected per the data sheet design, except the external thermistor is not loaded. The pack configuration register reads from flash = 8138.
2. Is the -v200 only a firmware change, or did the die change too?
3. If upgrading to -v200, does another golden file have to be created? Also, does the EVSW have to be upgraded also and where would you find that?
4. I've been struggling through lots of info trying to figure out how to program and calibrate the gas gauge outside of the TI software. It appears to be painful. Our production will not allow out of house software on the production floor. Is there a more streamlined approach to this? I've read all the app notes associated with the product. I would also like a prelim copy of the tool that allows creating a bqfs and a dffs file with an encrypted record (senc) and optional file containing the specific Data Flash Image (DFI), from SLUA541.