Hi,
many power, MCU etc. ICs have VCC max 5.5 V (6 V absolute maximum rating). Is it good practice to connect these ICs directly to USB bus power? USB states 5.25 V max on the bus, which complies with ICs rating, but my feeling is there is only a small reserve to reach ICs max rating....
Thanks for your comments.