Hi dear friends,
after solving a problem with the power factor what I saw is that the mosfet I was using (FCD4N60) that looks better than the one used in the EVB is overheating, in few minutes is reaching more than 120C at room temperature of 20C. The mosfet has a good dissipation pad and there are not other components overheating around it. I replaced it with an IPD65R190C7, that is a super mosfet with really good characteristics and the result is the same. I think the problem is not the current (measured about 100mA in RCS) as it stands 8 amps without problems. The voltage that stands is 650V and I'm powering the device at 115VAC. What can it be??
Thanks in advance.
Miguel