Other Parts Discussed in Thread: BQ3060, BQEVSW, EV2400
Hi,
I'm having a problem with BQ3060 where the cell voltages are really off.
I measured 2900mV and the bq Eval sw reports 3600mV.
That's a lot of discrepancy. I have not performed any voltage calibration, but I was under the impression that this was factory calibrated to 10% error.
I can live with 10% error, but this is quite a lot of difference.
It's causing my cells to be extremely depleted and the chip performs very erratically. The charging FET doesn't turn on anymore and I had to force a cmd 0x46 data 0x0006 to turn it on and charge the cells again.
But then, the reported values for all cells also wrong when charging and went well above the 4200mV. I knew there was no danger to the cells, because the actual values were around 3900mV.
What could cause such a discrepancy?