Other Parts Discussed in Thread: UCC28070A
I am looking for an interleaved boost PFC controller to supply 8KW, What controller would be a good choice?
Input AC: 480-575 VAC single phase
Output DC 800Vdc at 100A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCC28070A
I am looking for an interleaved boost PFC controller to supply 8KW, What controller would be a good choice?
Input AC: 480-575 VAC single phase
Output DC 800Vdc at 100A
The UCC28070A is an interleaved CCM type pfc controller and you should consider using it in such an application. The resistors sensing the input AC and the DC output can be scaled for the high voltages in your design. The UCC28070A ha a lower frequency limit of 10kHz which makes it suitable for driving IGBT's
Regards
John Griffin