This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX16993 replacement

Other Parts Discussed in Thread: TPS65261, TPS54302, LM53635-Q1

Hi Sir,

I am looking for a device to replace MAX16993.  I got the information from TI web cross reference that TPS65261 has similar functionality with MAX16993.  I need a device which can support higher input voltage up to 28V. Does TI have any suitable solutions? Single chip or discrete solution (two chips) are ok for me. 

Thanks!

Vito