Hi team,
When my customer is using BQ24610, the input adapter is 24v, the Vbat setting is 7.4v(two series battery), we can get the PACK+ has current, But when we set the Vbat to 23v, (5 series battery equal to 21.8v)we cannot detect the PACK+ current.
we test the status 0 and status1 are high logic.
VCC is 24v, HDRV keep 22v, LORV keep 0v. REGN=6V.
So i guess it has connection with the Dmax of the BQ24610. Do you have some suggestions?
Thanks.
BR
Frank