Hi Team,
In BQ76PL455's datasheet, for passive balanced, the recommended circuit has a series of 2K resistors in the MOS gate, and uses the 100K resistor to pull down between the source and the gate:
1, why use such a large resistance 2K and 100K , what are the considerations?
2. Is it possible to use the 100 resistor instead of the 2K resistor ,and use the 10k instead of the 100K resistor ?
在BQ76PL455的datasheet中,关于被动均衡MOS的驱动,推荐电路在MOS的栅极串联了2K电阻,并使用100K电阻在源极和栅极之间进行了下拉,请问:
1、为什么使用2K和100K如此大的电阻,有何考虑?
2、是否可以使用100Ω电阻代替2K电阻,使用10K电阻代替100K电阻?