Other Parts Discussed in Thread: TL431,
Hi,
I have created a circuit to power SSLT2 using TPS 53317A.
My circuit has problems.
Since the DCDC Buck on the input side of TPS 53317 A can not be sink, the input voltage (2.5 V) of TSP 53317 A increases.
I am considering the following contents to solve the problem. Is there a problem?
1. Increase 2.5 V to 3.3 V.
2. Connect TL431 (2.5 VREF) to 3.3V.
3. The REF voltage (2.5 V) of TL 431 is divided to 1.25 V at 10 kΩ.
4. Input 1.25 V to the REFIN pin.
Best Regards,