Part Number: LP38691-ADJ
Hello,
I have a serious problem with limitation current of the device.
On an actual PCB we use LP39681-adj LDO regulators, and I have problem with them...
Current limiting doesn't work anyway, if I short output or if I connect an empty 20µF capacitor,
I have a current (peak) of 1.3A (!!) instead of the 850/350mA limitation given in the documentation....
input power supply do not accept such current and all the other alimentations of the board are shut down !!
On simulation I have correct currents but in real life I don't have them....
Why do I have such current on output ?
Thierry