This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ501210: BQ501210's FOD configuration

Part Number: BQ501210

Hi,

BQ501210's FOD configuration issue. There are 4 pins related to BQ501210’s FOD debugging.

Pin 19 (FP_GAIN): Output to select the FOD ping calibration gain

Pin 20(FP_OFFSET): Output to select the FOD ping calibration offset

Pin 22(FOD_CAL): Output to select the FOD calibration

Pin 23(FOD): Output to select the foreign object detection (FOD) threshold

 According to the specification, the external resistance of these four pins is configured. And the threshold resistance is adjusted according to the FOD threshold configuration table (table1), but the result is not satisfying.

Could you tell me how to configure the resistance of the other 3 pins?