Other Parts Discussed in Thread: TPS730
Hi,
1. The TPS736 datasheet have the separate specification for current Limit and short circuit current. But in many other datasheet have only current limit. I feel in TPS736, short circuit and current limit is different.
Below sharing my understand on this, please correct me if my understanding on this is wrong.
A): At Current limit condiction : Output voltage will be stable (3.3V in the case of 3.3V LSO) and current will be same (Limiting current of Max of 800mA) even though the load varies.
B). Short Circuit condiction: Output voltage will be zero and current will be settle to 400mA (typ) .
2. First Test condition for current limit is Vout=0.9xVout(nom), please let me know, how this condition is achieved since the output voltage of LDO is fixed ?
Vout(nom) : Is the typical value of LDO output (3.3V in case of 3.3V LDO) ?
Regards
Anuraj NK