Part Number: UCC3895
Other Parts Discussed in Thread: UCC2895, LM5046, UCC28950
Dear colleagues,
we use the UCC3895 (UCC2895) for a high voltage source with an input voltage of 360V DC.
The output transformer has a high winding ratio (from 360V to 10kV), so with the lowest level shift from the controller,
the output voltage at light loads behind the full bridge rectifier is always to high (600V DC).
Is there a possibility to reduce the minimum level shift or skipping pulses like burst mode?
Maybe I have to switch to an other controller to get the output regulated.
Thanks for your help.
Frank