This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4132: Load Independent 5mA constant current source (Load Resistance 650 ohm to 750 ohm).

Part Number: LM4132

Hi, 

We are looking for Load Independent constant current source, Load current value will be 5mA. Load resistance will vary from 650 Ohm to 850 Ohm. Input power is 5V.

Also, it should have lower temperature coefficient, because this is going to be implemented in Sensor application.

I do have size constraint on board,  so I am looking for less component solution. While working on TI website, I found following design.

Will this work as Load independent ( 650R to 850R) 5mA constant current source?

Thank you,

Regards,

Rajesh Matere.