Other Parts Discussed in Thread: LM324
Hello Sir,
I have used all components as specified in datasheet only. I have used R1, R2 values,which are derived from Formula as mentioned in data sheet.
Input voltage range: 22V-30VDC
Output voltage=21V
Output current=1A
Load for the circuit is battery. I am using circuit as battery charger.
I am getting desired output voltage of 21V. It is clearly mentioned in data sheet of IC that its of 1A.
The problem I am facing is that whenever load draws current more than 1 A, IC does not restrict it. Current supplied by IC goes upto 3A, after which IC Heats up and goes into thermal shutdown. After which output of IC goes to 0V.
Please help to resolve.
Dushyant