Other Parts Discussed in Thread: TPS62823
Hi,
Please let me ask about maximum output current. I know that the maximum output current depend on input and output voltage, but I'm asking it because the maximum output current of efficiency curve in datasheet is 2A. The actual requirement of the customer is 2.3A output current at 2.5V output from Li-Ion battery (3.0V to 4.2V). I could get result without no error from Webench as attached.
webench_design_964463_1036_258173640.pdf
Best Regards,
Satoshi / Japan Disty