This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM350A: 5A Constant Voltage/Constant Current Regulator

Part Number: LM350A
Other Parts Discussed in Thread: LM358

Hey,

we are working in a group of students, from the Technische Universität Berlin, on a battery project, using the LM350A for the battery charger.

We are using the circuit "5A Constant Voltage/Constant Current Regulator" from the datasheet (Fig.29).

The circuit is not running, as we would wish or expect.

For example:

With a battery load voltage of 3.5V, the battery current and the total input current of the circuit have almost the same value.

So we are losing about 90% of the electric Power from the 35V-Input to the battery (3.5V).

We do not understand this behavior of the circuit. So could you please give us some extra ducumentation for the circuit from the datasheet.

On more question:

Is it possible to replace the lm301 by the lm358. The special impact of the lm301 is also something we would like to understand better.

Thanks a lot!

  • Hi Johannes,

    LM350A is a linear regulator. As such Iin = Iout + Ignd. With a high Iout, Ignd is negligible; therefore, Iout will be roughly the same as Iin. As such efficiency will be roughly Vout / Vin x 100. For greater efficiency you may want to consider a switching regulator to step down the voltage before the linear regulator.

    LM301 was simply used as an example, any amplifier can be used so long as you adjust the bias rails accordingly.

    Very Respectfully,
    Ryan