Other Parts Discussed in Thread: , TPS61230
Hi team,
Is the LM2623 can be used for Vin 3~4.2V and output 4.1V, 1.5A?
I'm not sure that can support 1.5A at 4.1V or not.
Also, another question is that the LM2623-Q1 need VDD= 3~5V.
Our application is Li-on battery(3~4.2V) for Vin and can I connect Vin and VDD together?
And the LM2623-Q1 can support output 4.1V at 1.5A?
Thank you!