Could you please let me know in more details how to adjust the Output Voltage to 1.35 v given that the Vin is 3.3v?
Voltage Reference and Adjusting the Output Voltage
The voltage reference system produces a precise ±1% voltage reference over temperature by scaling the output
of a temperature stable bandgap circuit. The FB voltage is regulated to the voltage reference. The output voltage
is set with a resistor divider from the output node to the FB pin. It is recommended to use divider resistors with
1% tolerance or better. Start with a 10.0 kΩ for the bottom resistor RFBB and use the Equation 1 to calculate
RFBT. The maximum recommend resistance value for the bottom resistor is 100 kΩ.