Hi,
I bought the LMG3410-HB-EVM Half-Bridge and LMG34XXBB-EVM Breakout Board EVM. I'm trying to use parts of these to build a pcb of my own. The altium files online seem to be read only, and I don't have access to the pcb libraries or schematic library. Specifically, I was wondering I could be provided the libraries below, since I'm trying to save some time, and building these connectors on my own may be risky. (If it's easier I could search through all the files you have for these two parts and find it myself.)
Libraries/part:
Connectors_Mill_Max.IntLib
Connectors_Molex.IntLib
Pin Receptacle, .032-.046" .075" Dia, Gold// TH 0312-0-15-15-34-27-10-0// Mill-Max
Receptacle, 2.54mm, 6x1, Gold, TH 448120024 Molex
Thanks!
Harish