Hi
I was looking at the datasheet of the TPS736 and specially the typical application section it says that there is a minimum of output current (20 mA for the fixed voltage version, 10 mA for the adjustable). I read about it but I didn´t find a good answer to keep forward in my design, because my sensor needs 1.8V (fixed voltage version could be better) and the typical current load is 10 mA (below that level). I want to know if this is important for the functionality (stability, noise,..) and in that case if I should connect a small resistor to sink or load some current or replace the regulator for other one pin to pin compatible.
Thank you