Hello team,
my customer is using the LP5030 and noticed something about the address of the broadcast.
At page 21 of the datasheet, on table 2. Slave-Address Combinations, it shows that the IC can be configured with the addresses 0110000, 0110001, 0110010, 0110011 and it has another address for the broadcast 0011100.
I would like to get a confirmation on the address for the broadcast; I hope it's not with the first part similar to the configurable addresses, because they would like to use 4 devices of LP5030 on the same bus which has an address 0110100, that happens to be the broadcast address with the higher part similar to the configurable addresses.
I'm asking just to be sure, otherwise the whole board would be unusable.
Thank you and best regards,
Adrian