Other Parts Discussed in Thread: LM5145, CSD19533Q5A
Hello guys,
One of customers is evaluating CSD19534Q5A with LM5145. But they is serching for any MOSFET which has shorter Td(off) and tf than CSD19534Q5A (Td(off)=20ns, tr=6ns) because LM5145 dead time
between low side MOSFET=on->off and high side MOSFET=off->on is very small (14ns).
Could you please tell me that any NMOSFET which meets the following condition?
VDS =80V~100V
ID=30~50A
VGS=+/-20V
RDS(on)=less than 20mohm
td(of)=less than 20ns
tr=less than 6ns
Ciss=less than 1300pF
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.