Hello,
Posting on behalf of my customer.
Based on the package options in the datasheet, the TPS53317A is rated up to 125C operating temp. However, when creating a new design in Webench Designer it limits me to 85C so I cannot check if this part will work in my design. I plan to run it at 100C ambient. Will this device work? I'm planning to use it at 6Vin, 0.6V out, at 6A. I need to understand if this part will support my DDR4 application.
Please help.
Thanks,
Tom