Other Parts Discussed in Thread: UC2907, UCC29002
Hi there,
Assume an isolated dc/dc module with 53 V input voltage, 28 V output voltage, 25 A output current capability and remote sense pins. I would like to parallel two of the module to meet high load current demand. It seems that UC2907/UC3907 can be a good candidate for this purpose. I visited TI's website very carefully and found many technical documents. Of course they are excellent, but there is no document to have real example with details of calculations. I'm just wondering if anyone has such an experience that can share with me.
Thank you very much in advance!
BR,
Ghasem