This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5024: LED RGB color and min out

Part Number: LP5024

Hi Sir,

May I know what is the min Vo , from the Fig.7 of LP5024 datasheet, is 0.5V ? for example, if LED voltage =2.6, the min VLED is 3.1V.

  Secondly, we do the experiment and found out the color will be different when Rref change but in same current setup. For example as below, the color is different, would you please help to share is it normal since we don't have much experience in RGB LED control 

RIREF =2.2k with 6.5mA (adjust ADC to get 6.5mA)

RIREF=11k with 6.5mA (adjust ADC to get 6.5mA)