This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS736-Q1: 3.3v/300mA/SOT-895 LDO device requirement

Part Number: TPS736-Q1

Hi team,

This is Jessica, glad to work with you.

Could you please kindly help to recommend a LDO. The detail requirements is 3.3V output voltage, 300mA output current, and the package is SOT-895 for Automotive. Since i can't found this kind of package device in TI.com, so could you please kindly help to confirm if we have suitable device can be recommend to customer? Thank you very much for your support.

Best regards

Jessica

  • Hi Jessica,

    Thanks for reaching out to us about this. You are correct that we do not have a SOT-89 package in automotive. Would you be able to provide some more requirements for the application? It seems from the part choice that you have a low Vin application, but do you have any more information about noise, psrr, and transient requirements? It would really help to narrow down the parts. Without any more requirements it looks like you have picked the best part.

    Regards,

    Mark

  • Hi Jessica,

     

    Since it has been a week without a reply, I assume that this thread is resolved. If this is not correct, please feel free to post again.

     

    Regards,

    Mark

  • Hi Mark,

    Sorry for this late reply and thank you very much for your support.

    After confirm with customer, they think TPS736-Q1 also can reach their requirement. Thank you again.

    Best regards

    Jessica