Other Parts Discussed in Thread: TPS2120,
Hi E2E,
we would like to use the TPS2113 in an environment where IN1 is connected to a DCDC converter (2.5A) and a Li-Ion battery on IN2. The output drives a CPU someperiphals and a GSM modem. This modem draws in transmit mode worst case up to 2.5A for a duty cycle of 12.5%. The overall, with CPU and some other peripherals, current would be 2.7 to 2.8A in transmit mode and 200-300mA in receive mode of the modem.
I've checked the datasheet and on average we neither hit the 1.25A current limit nor the dissipation ratings.
- Can you recommend this part for those operationg conditions?
- Anything else to consider if we want to use this part in this environment, like setting the Ilim correctly?
- The figure for "Current limit settling time" suggests that 577us should not be a problem, correct?
- I've already checked some other devices from your portfolio, but e.g. the Iq of the TPS2120 is too high. Any other solution you can propose?
Thanks and best regards
Stefan