Other Parts Discussed in Thread: TPS546D24
I want to design a dual power system. The two power supplies are 1+1 redundant backup. If one of the power modules is unplugged, the other module works normally. Each power module needs to supply 5V/50A current. If each module uses two TPS546C23, can the output of the four TPS546C23 in two modules be connected together ? We need load balancing.
If 4 X TPS546C23 can't be stacked, is there any good solution?