Other Parts Discussed in Thread: TPS7A05
Hello,
I noticed on CC1312 Lanchpad, the TPS79601DR programming resistors sum up to 81KOhms which wastes 40.7uA continuously?
- Can I keep the same resistor ratio but increase their values? i.e: instead of 51K and 30K, I use 510K and 300K for example?
- What is the limitation on the values of these resistors?
- The Compensation capacitor value will decrease (according to the equation 3 in page 16 in the datasheet http://www.ti.com/lit/ds/symlink/tps796.pdf
Thanks