Other Parts Discussed in Thread: UCC27712, UCC27712-Q1
Hello, I have designed motor control power stage for 20 years. Recently I had to deisgn a 1.5KW stage for a brushless DC motor as per I did before. This is the first time I use the UCC27212 driver. For the last 2 weeks I burnt 15 pieces just by starting my power stage while the current involved is as low as 0.5 A under 20VDC and the dead time high enough to make sure there is no cross conduction (that I checked with isolated probes). After 2 weeks of intensive unsuccessful trials I must admit there may be something wrong in the inner part of this device. As an example, when I even output a fixed duty on a light load, after 1-2 trials (start-stop-start...) the device get burnt : the low side is shorten internally and I have to replace it. I am sure of my layout (that I can share with you), I am sure of the connections, I am sure of the wiring. I tried different decoupling capas -> no change, even I tried to change the bootstrap diodes (and without) -> no change, I changed series gate resistors with higher values to slow down dv/dt -> no change.
today I replaced the ucc27212 with legacy drivers from competition (l6386), all good.
I am keen on using the UCC27212 as the datasheet looks outstanding, but to me there is a design or quality issue. Have you suffered any production issues on these devices? I could see that some distributors dont hold any more stock of these devices (Farnell for example). Is the 10 pin package with pin to pin spacing the issue? Do you have a reference design with proven motor control stage working at 2-3kW with these devices?
Thnaks/Florent