Hi,
I am using step-up converter TPS61240DRVR to step up 3.7V from the battery to 5V which is required for my application. I referred datasheet and made a schematic, after getting PCB, it was working for around 3-4 months until suddenly other day battery become swollen. The device was with the software team who have no idea about hardware immediately disconnected the battery and left it over.
After disposing of the battery, I took the fresh battery and connected it to the board after found that the board was heated and found the step-up converter was very hot. I removed the battery, took a new board and connected the battery but again it was hot on the new board.
I thought it must be a battery issue, changed a battery again, tried previous battery on some other application board and battery was working fine. I have a single side battery input connector so there is the least possibility I might have connected the battery with the reversed polarity.
Also do I need to pulldown EN pin to ground with pulldown resistor as it is enabled and disabled form microcontroller pin for now?
What could be a possible reason for the same?
Can you please let me know how to debug the issue?