Other Parts Discussed in Thread: LM25066
Hi Team:
it is known we will propose customer to use a clamped TVS to suppress the voltage energy when transient or hot wrap activity occurs, However, some Practical running results shows that once the TVS is failed to be short potentially, the end customer's system will shut down by the 12Vin BUS, which is a fatal system problem, end customer can let one rail of the 12V Efuse(LM25062/6) to be open when failure occurs but not affecting the 12Vin BUS's other server boards, so, end customers has great worry on the use of TVS at the front of Efuse (LM25062/6)side.
So, the problem we face is :
if TI customers want to discard using TVS at the front end of LM25062/6, do we have other solution to fix the original issue? or if we do not have the good solution and just delete TVS, Can we promise that LM25062/6 is safe during the worse case?
can you help to check if it is possible in the case that customer may switch to other competitors and there is no TVS.
Thanks very much!