Hi,
We plan to create a 9V output from a 12V input using TPS7A24.
Please tell us the recommended resistance values for R1 and R2.
The minimum value of the input voltage is 10.8V,
the load current is typically 50mA and the maximum is about 110mA.
Best regards,