This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55010: Is TPS55010 feasibly for customer requirement?

Part Number: TPS55010

Hi, team.

i've been asked by Customer as below.

is TPS55010 feasible below customer requirement ?

temp range:0~100℃

load :0~180mA

output voltage :±5%

Input 5V

output:9V

what if customer does feedback from 2ndary , will it be feasible ?