Hi team,
It looks like the datasheet of TPS62363 has vague description about register TEMP.
The datasheet states " If the device's junction temperature, TJ, exceeds 120°C typical, the TJEW bit is set high. " and " If a thermal shutdown has occurred, the TJTS bit is latched and remains a logic high as long as VDD and AVIN are present and until the bit is reset by the host. " So, I think it means the TJEW bit can't be writen by users while the TJTS bit can. Am I correct ? If so, when I program the register TEMP by I2C, I need to place 8 bits data on the SDA line, does this have any side effects on the TJEW bit ?
Regards,
Noah