This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61240-Q1: Ripple voltage more for TPS61240

Part Number: TPS61240-Q1
Other Parts Discussed in Thread: TPS61240

Hello,

I have ordered evolution board of TPS61240 I am testing it using 100mA Load my power supply showing the drawn current is of 160mA I am using Electronic load as a load it can detect the Current of 100mA so is that TPS61240 taking extra 60mA Current ??

also I have checked the Ripple voltage at the output it is 180mV is it really that much or I am missing something ??

Thanks in Advance !!!