Other Parts Discussed in Thread: TPS54824
Hi Sir,
Coulde I use TPS53513 in the applacation as below:
Vin=5V Vout=4V Iout=3.5A
The concern is could TPS53513 handle the big duty cycle? the worst case should be at the start up.
and also there is a 5V LDO inside, if the input voltage is below 5V, could the Vreg supply for the device and the gatedriver?
If TPS53513 can't support this application, could TPS54824 support? this one suport 100% duty cycle.
Thank you very much.