Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS542941: quiescent current and shutdown current

Part Number: TPS542941

Hi 

The datasheet specifies the Vin current is 1300uA (condition EN1=EN2=5V, VFB1=VFB2=0.8V) 
1. Does it referring to non switching condition?
    If not, what is the quiescent current at non switching condition?

2. Could you explain the reason of shutdown current 80uA which is relatively high? 

Rgds
Kelvin

  • Hi, Kelvin

    1. Yes, it is non-switching condition.

    2. Confirmed with designer, when EN1=EN2=low, some internal circuits(including bandgap reference and bias circuit) are active, so the shutdown current is a little big.