Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100
Hello,
we plan to use the BQ34Z100-G1 with 80Ah 18650 LiFePo cells.
As the production process should not be too complicated, we would like to use the IC directly and only change some parameters in the config of the device. These changes will be done by our series microcontroller using I2C, without any bqStudio or computer connection in the test-bench.
Is it correct that the "chem ID" is something that is only in the BQ software and is not written to the device itself somewhere? Do we just leave the register "device chemistry" at "LION" and modify some of the settings like the "design capacity" and "design energy" and the "pack configuration"?
Is this possible, not using any fancy Software, golden image, ...? Would a learning cycle be performed automatically for each Battery once it is used first?
Is there an overview available, which registers we should modify upon first-time usage?
thanks,
Michael