Other Parts Discussed in Thread: UCC28050, UCC28051
Hello:
according to your recommended PFC management chip, after reading the information carefully, I found that the data recommends that the crossover frequency of the compensation circuit (loop) be set below 20Hz. After reading the relevant information, I know that the input is a power frequency AC at about 50Hz ~ 60Hz (to achieve a high power factor ratio).
Then if my power input is AC from 360Hz ~ 800Hz, can I set the crossover frequency to 32Hz ~ 100Hz or higher in proportion? UCC28056's internal circuit is not limited to the frequency bandwidth, or the algorithm is not suitable for higher input frequencies.
Question 1: Are all the PFC management chips of TI the bandwidth is less than 20Hz.
Question 2: Is this bandwidth an inherent design of the chip's internal circuit and cannot be changed externally?
Question 3: If you are convenient, I hope to explain to me the relationship and principle of this bandwidth or crossover frequency setting and the input AC frequency. Related materials are also available.
Question 4: Please help me recommend a wide bandwidth PFC management chip, or it can adapt to 360Hz ~ 800Hz input.