Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138HSFBEVM-029: Power management forum

Part Number: UCD3138HSFBEVM-029
Other Parts Discussed in Thread: UCD3138064

Tool/software: Code Composer Studio

Hi everyone, i need to generate dpwm waveform ,for this i have referred videos in ti website, but couldn't able to get dpwm waveform.  Could you please tell me is there any necessary hardware connection get dpwm waveforms. I have atttached the code, is there any changes to make in code?

[code]

#define MAIN 1
#include "system_defines.h"
#include "Cyclone_Device.h"
#include "pmbus_commands.h"
#include "pmbus_common.h"
#include "pmbus_topology.h"
#include "variables.h"
#include "function_definitions.h"
#include "software_interrupts.h"
#include "cyclone_defines.h"
#include "stdio.h"
#define PCLK_PERIOD         4.0e-9
#define PERIOD_SECONDS      10.0e-6
#define PERIOD_CLK          ((int)(PERIOD_SECONDS/PCLK_PERIOD)<<4)
#define EVENT1              (int)(PERIOD_CLK*0.00)
int ram_event2;
void inti_dpwm(void)
{
    Dpwm0Regs.DPWMCTRL0.bit.PWM_MODE = 0;  // Set to normal mode
    Dpwm0Regs.DPWMCTRL0.bit.CLA_EN = 0;
    Dpwm0Regs.DPWMPRD.all = PERIOD;
    Dpwm0Regs.DPWMEV1.all = EVENT1;
    Dpwm0Regs.DPWMCTRL0.bit.PWM_EN = 1;
    LoopMuxRegs.GLBEN.bit.DPWM0_EN = 1;
}
void main()
{
  
    if(GioRegs.FAULTIN.bit.FLT3_IN == 0)// Re-Check pin assignment (ADC_EXT/SYNC may be?)
    {
        //clear_integrity_word();
    }
#if (UCD3138|UCD3138064)
    MiscAnalogRegs.CLKTRIM.bit.HFO_LN_FILTER_EN = 0;
    MiscAnalogRegs.CSTRIM.bit.RESISTOR_TRIM =23; //28;
#endif //(UCD3138|UCD3138064)
    init_pmbus(0x58);
    init_dpwm();
    ram_event2 = Dpwm0Regs.DPWMEV2.all;
    for(;;)
        {
            pmbus_handler();
            Dpwm0Regs.DPWMEV2.all = ram_event2;
        }
    }

[/code]

Thanking you.