Other Parts Discussed in Thread: BOOSTXL-TPS65218, LP87524-Q1
Hi Team,
Customer is evaluating one PMIC from other vendor, general specs are as follow:
5 Regulator Rails for 4 Buck Converters and 1 LDO
CH1 : Buck, 0.6V to 1.39375V with 6.25mV/Step,Output Current : 3A
CH2 : Buck, 1.1V/1.2V/1.35V/1.5V Set via External Resistor, Output Current : 2A
CH3 : Buck, Fixed 1.8V, Output Current : 1A
CH4 : Buck, Fixed 3.3V, Output Current : 2A
CH5: LDO, Adjustable via Resistor Divider, Output Current : 400mA
Based on this, could you recommend a suitable solution to compete with this?
Thanks and best Regards,
Will