Hi
TPS7A4901DGNR: what's the Vout(nom) value in Vdo item?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Max,
VOUT(NOM) is the target regulation voltage. Meaning if VOUT was set to 5V, VDO is measured with VIN = 4.75V and with a load current of 150mA, VOUT could be as low as 4.15V (5x0.95-0.6=4.15).
I hope this helps to clarify.