This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27212: Switching characteristics

Part Number: UCC27212

Good day!

I have some question about information in your datasheet  for device UCC27212.

Datasheet provides some information about dynamic parameters on pages 7-8 (cf. section 6.6 "Switching characteristics").

According this information, test condition is VDD=VHB=12V or VDD=VHB=6.8V. I haven't found any information about input voltage.

What is the input voltage for this dynamic parameters?

Best regards 

  • Hello Mark,

    Thank you for the interest in the UCC27212. I did look at the datasheet and I see why you ask the question.

    When you mention input voltage, do you mean the peak voltage on the LI and HI input pins? I assume that is the case. Please confirm if that is the voltage you are referring.

    I need to confirm to be certain, but I think the test conditions are with 5V peak on the LI and HI inputs, it may be 3.3V peak.

    Confirm if this addresses your question, or you can post additional questions on this thread.

    Regards,